LM5145 手册标的能到99%占空比,实际占空比到不了99% 48V输入只能47V输出,带载10A后降到46V。占空比只能96%不到。是什么原因?用凌特的IC就可以到99%占空比。电路图见附件LM5145 DEMO.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM5145 手册标的能到99%占空比,实际占空比到不了99% 48V输入只能47V输出,带载10A后降到46V。占空比只能96%不到。是什么原因?用凌特的IC就可以到99%占空比。电路图见附件LM5145 DEMO.pdf
HI
注意一下你的频率,同时一般最大duty是要大折扣的,因为理想状态下100%效率。
你可以算一下,即便100%duty, 输入到输出,也要经过电感和MOS,电感DCR, MOS Rdson, 10A电流,产生1V的压降差不多,