求推荐款:输入电压为9--54v,输出为5v,输出电流在4A左右,可以并联输出,具有反向电流电压保护一分钟以上,快速瞬态反应
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
就你的应用而言并不需要用到同步,因为是给不同的负载供电,可能只是时序有要求,应该是不会要求绝对同时电压输出。
如果是这样的话你可以选择TI的TPS54360: http://www.ti.com.cn/product/cn/tps54360 这个芯片最大输出电流时3.5A, 可以给MG323供电, 另外在采用同系列的TPS54160: http://www.ti.com.cn/product/cn/tps54160 给另一个5V供电,同时由这个5V再产生一个3.3V. (如果是独立的供电,并不会造成反向电压。)
TI即将推出的同系列芯片TPS54560是可以提供5A输出电流的,这样就可以采用一个芯片实现。
如果采用外部MOS控制器,则符合的很多,如LM5088,LM5117, TPS40117等等。