This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220输出问题



你好,TI。

这个片子用做锂电池(2.7V-4.2V)升压再给产品供电。

要求稳定持续输出5.2V,峰值电流至少95ma。

为什么不能通过webench的设计。

我看参数是1.8V可输出0.4A,那么输出5.2V应该支持到0.138A。那里有不对的吗?

临时飞线了个电路,在负载为1ma电流时,效率只有62%。

这个哪里可以改善,外围的容阻和电感要贴的非常近吗?