TPS63001电流问题,现在使用TPS63001做升压测试,电源输入使用2节5号电池,发现在没接负载情况下,电流竟然达到6ma,请问这可能是什么问题引起的?电路图按照手册搭建的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS63001电流问题,现在使用TPS63001做升压测试,电源输入使用2节5号电池,发现在没接负载情况下,电流竟然达到6ma,请问这可能是什么问题引起的?电路图按照手册搭建的
Hi
按照datasheet静态电流的测试条件: IO = 0 mA, VEN = VIN = VINA = 3.6 V, VOUT = 3.3 V, 静态电流将是50uA左右。
事实上如果要得到如此低的静态电流还需要芯片工作在PowerSaving的模式下,即PS/SYNC接GND。 如果是工作在PWM模式下,静态电流确实可能是6mA左右。.
如果你采用的是升压控制,也是可以的,电路可以参考datasheet第一页,将PS/SYNC接GND。
的确是这样,再问下PS/SYNC使能和失能有什么区别?
Hi
PS/SYNC接GND, 芯片工作在PowerSaving的模式下, 这个是为改善轻载效率的,也可以得到较低的静态电流。
PS/SYNC接VCC, 芯片工作在PWM模式下(定频DCM模式),轻载效率比较低。