This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ34Z100-G1 IIC读取参数的问题

Other Parts Discussed in Thread: BQ34Z100-G1

您好,我在使用BQ34Z100-G1做电量估算时出现了如下两个问题,暂时没有找到原因,应该是偶现,也不太好复现,请TI帮忙分析下会是哪里的问题:

①我的电池6S在瞬间大电流放电时(如>120A),个别电池在1分钟左右SOC显示0%,应该不是读取的问题,我怀疑是放电到了Cell Terminate Voltage,我适当降低了一些这个值,好了一些。但还是会出现,如果是这里的问题,是否会影响SOC估算。电芯放电截止电压3V,我已经改为2.5V了。

②我是GPIO模拟的IIC,这里偶尔会读出一两个错误的值(有时是温度,有时是电压),比如1s更新一次,跑了20天,出现了两个电压错误,如下图,这个状态不好抓取,请帮忙分析下是哪里出了问题。谢谢。