Other Parts Discussed in Thread: TPS54360, TPS5401
频繁开关电源输入,buck 芯片启动的有声音,不是电感和其他器件,声音频率与开断电源的频率相同,所有的芯片外部器件都去掉后仍然有,试验过tps5401,TPS54360,现象都一样, 是芯片自身的声音,不知道原因
电路参数在DCDC长时间工作时,是没有声音的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的用法是这样:需要3Hz闪烁的灯光,实现方式是控制灯光的供电电源(只能用这种方式),现在,用TPS5401芯片 做了以下试验:
1、用设计好的电路,测试电源输出稳定,一直通电,没有异响;
2、采用闪烁的模式,发现电路声音;
3、补焊了芯片的底部的散热焊盘,闪烁模式下 声音一样;
4、去掉电感和电容,闪烁模式下声音存在;
5、把芯片外围的所有器件全部去掉了,电源芯片的SW脚在通/断电的时候,就有一个脉冲输出,声音存在;
6、关闭EN断,也有这个脉冲,声音存在;
7、用一个设计好的TPS54360电源模块,按3HZ的频率闪烁(如果滤波电容大,需要降低频率),也同样有这个声音,还有一片其他公司的DCDC模块,也是同样的现象;
8、电路我通电了一周,在闪烁模式下,除了有声音,电路工作正常,
现在,不能确定这种工作模式下,这个电源电路是否可以长期稳定运行,如何可以把这个声音消除