This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562201输出电压不正常,会随输入电压变化



使用的是TI官方电源设计软件生成的电路,和数据手册的典型应用电路对比也差不多。按输入12V,输出5V设计,一个10K和一个56.2K的电阻,理论输出应该是

0.765*(1+56.2/10)=5.06V,实际输出4.23V。用的是直流稳压电源作为输入来测试,此时工作电流是50ma左右(是不是太低了?)而且调低输入电压到9-11V时,输出电压也跟随着显著变化,最低会降到1.8V。试过把输出很后端的电路断开测试,结果接近。

这款芯片的输出电压不应该是固定的么?请问可能是什么原因导致的?