最近在使用TPS63806这个升降压IC驱动LED时,输入为3.6V,输出在3.7V,需要3.2A。FB脚加R(24K)C(1uF)+8K PWM,通过调节PWM占空比来调节IC的输出。当直接将R与MCU连接的一端直接连接GND(0%占空比)时,IC输出可以达到3.4A。但是当使用MCU输出一个8K 的占空比,从30%调至0%,输出始终是2.7A,非常着急,请求TI工程师支援一下,该怎么解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在使用TPS63806这个升降压IC驱动LED时,输入为3.6V,输出在3.7V,需要3.2A。FB脚加R(24K)C(1uF)+8K PWM,通过调节PWM占空比来调节IC的输出。当直接将R与MCU连接的一端直接连接GND(0%占空比)时,IC输出可以达到3.4A。但是当使用MCU输出一个8K 的占空比,从30%调至0%,输出始终是2.7A,非常着急,请求TI工程师支援一下,该怎么解决呢?