上面是电路图,输出7.4v。因为驱动两个并联的MOS管,用TPS7A4001做了一个外接电源给LM25116供电,但是无法工作。4001正常输出电压8v,正常输出50ma没问题,接到25116后空载情况下测VCCX脚电压只有6v,VCC脚电压有时到7.4v,有时5-6v的样子,几十毫安的负载都带不起来,输出电压1v多,25116带载后VCCX电压降到1v多,VCC脚电压也下降厉害,输出也只有1v多,电感也响;尝试将VCCX接到输出,同样无法带载,输出电压降到1v多,电感响;但是将VCCX接地不使用,电路可以正常工作,带载十几安都可以。尝试将VCCX接到电源输出后VCCX输入电流33ma,空载和带载没有变化,好像超出了25116内部调整器15ma的输出限制,不知道什么情况,请大神帮帮忙。