最近用根据TPS23753A的芯片资料原理图lay了一块板子,在调试过程中有一些问题,求各位大大帮忙看下。
问题1:GATE引脚只有0.18V,开关MOS管Q2漏源极波形异常
黄色为正常波形,蓝色为异常波形,蓝色波形的板子输出有12V,请问是什么原因导致了这种情况
问题2:CTL引脚电压为2V。Vb引脚电压5V正常,Vc引脚只有6.6V,请问是不是因为Vc电压不足导致了问题1的出现
问题3:根据原理图的参数去调试,一开始没有输出电压,R13调整成100R,R11调整成56K之后可以输出12V,可是会出现问题1的情况
求大神帮忙看下,小弟初学者请见谅