This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无线LED照明系统的设计应用--硬件电路设计

Other Parts Discussed in Thread: CC1101, CC430F6137

3.1RF模块硬件电路设计

CC430的射频模块使用的是业界领先的不足1GHz的CC1101 RF收发器,该部分是基于RF频率的直接合成,其射频合成器包括一个完整芯片的LC-VCO和一个对接模式的混频器进行频率合成。该射频的接收单元将RF信号通过低噪声放大器(LNA)进行前置放大,再对其中频信号进行滤波、数据解调以及同步包等工作。CC430支持的频率范围为:300MHz~348MHz;389MHz~464MHz;779MHz~928MHz;在本设计中使用的是433MHz的载波频率,鉴于应用场合其要求的传输速率较低,因此选用的是3.2Kbps;并通过PATABLE对输出功率进行调整,不同的距离需求。RF模块的硬件电路在整个系统设计中尤为重要,如图3所示。

图中的C5,C9,L3以及L8形成一个平衡转换器,用以将CC430上的差分端口RF_N/RF_P平衡电路转换成单端不平衡的RF信号,方便将振子流过电缆屏蔽层外的高频电流截断。图中的L5,C10和L4构成了带通滤波器;L2,L6和C8构成低通滤波器。在本设计中RF的天线采用的是鞭状天线或者陶瓷天线。

3.2触摸滑条的硬件电路构建

在本设计中,控制端部分为手持式遥控模块。其设计的人机交互界面主要是LCD显示以及触摸按键。其中将触摸滑条的功能用于调节LED的亮度,是系统中较为形象与新颖的设计之一。其充分利用了MSP430的自身资源特性,在CC430F6137集成的比较器COM_B以及PCBLayout的传感电容上,构建了基于弛张振荡方式(RO)的触摸按键功能,由于在COMP_B中自带有REF参考电压配置网络,因此无需像COMP_A那样使用外部硬件方式实现参考电压网络。

其原理如图4所示,主要通过TimerA测量RC振荡电路在固定时间内的振荡次数,当人手触摸在传感电容上,会改变其自身电容值,使得对应的振荡次数发生明显变化,以此来判断触摸/非触摸的状态。构建一个4/5级触摸滑条与2个触摸按键。

3.3传感器硬件电路设计

光敏传感器的使用使得LED照明系统能够实现亮度自调节功能,硬件电路如图5所示。

光敏传感器使用的是光敏电阻,因其有着良好的光电特性以及价格优势,非常适合于光强检测场合的使用。系统中主要通过对Vo电压的检测,反映光强的变化,进而对PWM进行相应的调制。