Other Parts Discussed in Thread: UCC256402, UCC25600
你好,关于LLC芯片UCC256402这个芯片,我有以下几个问题:
1.起机频率怎么设定,最大能设定到多少。目前起机电流比较大,根据datasheet的说明取消了SS的初始化,起机频率在300k左右,但是频率很快就降下来了,起机电流还是很大。
2.最大和最小工作频率怎么设定?
3.burst模式下的开关频率怎么设定?
4.FB引脚的内部电流源只有91uA,反馈光耦的工作电流太小,有没有什么方式加大,通过RVcc上拉?
5.burst模式BMTH和BMTL的设定依据是什么,大小多少是合适的?因为看到BMTH建议是1~2V,但是demo板只有0.6V
6.如果工作过程中出现打嗝,可能是什么原因?详见如下波形,burst模式下展开波形,驱动好像在打嗝,相关保护都测过了,并没有触发