This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

多个BQ24650芯片可以对串联锂电池中的单个电池独立充电吗

Other Parts Discussed in Thread: BQ24650

单个锂电池,充电截止电压=2.6V,充电电流=2A,多节串联。单个BQ24650芯片设置输出电压=2.6V,充电电流=2A,单个BQ24650针对串联电池单独充电,这个电路可以不?如有问题,请明确指出,谢谢!

  • 应该是可以的,每个bq24650需要隔离电源

  • 每个BQ24650输入电源配置一个DC/DC隔离模块,输出DC24V,经过二极管到24650电源输入只有23.5V左右,我将MPPT电压设置为23V可以不?

     R11=1M,R7=56K,MPPT=22.6v?可以不?

    现在就是充电线路较长(约1米),导致电池电压=2.4V,在SRN和SRP端测量电压=2.55V,带来的问题是充电电流只有1A左右,达不到我要求的2A;将充电电压调高到3.2V左右,电流才能达到2A,请教,这个问题如何解决?