用bq24650做太阳能收集与管理,MPPT电压设置为5.5V,太阳能电池板开路电压7V,锂电池充电电压4.2V。
正常充电时,STAT1亮,STAT2灭,与datasheet里描述的一样。但是,电池充电到4.05V时,STAT1便开始有规律的闪烁,STAT2灭,不再为电池充电了,这是什么问题?STAT1闪烁,STAT2灭,代表什么状态?
还有一个问题,我参考官方设计设计的电路板,元器件全部和官方设计的方案一样。我设置的最大充电电流为2A,但是锂电池电压在3.9V以下时,太阳能电池板输出在5.5V,350mA时,bq24650的充电电流只有300mA左右,效率明显不对。采用外接电源的方式测试,输入12V,5A,充电电流也只有450mA左右,请问可能那些原因导致了充电电流这么低?