Other Parts Discussed in Thread: TPS65130, TPS65131
我现在再做一个电源,要求输入最大最为5v,输出为双通道的正负15v电压,电流要大于200ma,不知道专家你有没有哪一种芯片可推荐的,在这先谢谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
TPS65130(800mA)能满足您的要求,另外你也可以了解一下TPS65131(2A)。
请参考
http://www.ti.com/sitesearch/docs/universalsearch.tsp?searchTerm=TPS65130&linkId=1
改进了电路带载输出+-15V很稳,但是输入端电压(5V)受干扰太大,有0.6V的波动。