This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24172芯片无法充电问题

Other Parts Discussed in Thread: BQ24172

你好,我们选型BQ24172,输入电压14.7V,现在调试中出现无法充电,故障现象:
1、STAT状态灯闪烁
2、不挂电池时,SW输出12.6V【三节电池】
3、挂上电池后,SW端的的电压和电池电压一致:10.24V,STAT状态灯仍闪烁,在这种状态下,把电池移除,芯片的输出为0.5V,有时候是      0.7V左右。必须单板完全断电后,重启才能恢复12.6V输出。
4、测量了DataSheet中的相关参数为[挂电池]:VREF:3.3V  Iset:0.2V   Ovpset:1.3V   TS :1.94V    FB :1.70V  Vacset:0.2V
    TTC :1.26V   PVCC :10.24V  SRN :10.24  
麻烦帮分析下,谢谢支持
麻烦说明下,1、这种状态是芯片的哪种保护状态?在DataSheet中哪个单节有该问题描述?
                         2、硬件如何解决【硬件电路参数BQ24172的标准电路】?