This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TPS61165问题--6串3并350mA



各位好,第一次接触LED驱动,信心很是不足,总感觉有很多概念掌握的不够扎实,想请各位专业人士帮忙参考一下。方案电路图如下:

问题1:因为不需要调光,CTRL引脚可以直接接输入电压吗?因为我看到数据手册上有个R(ctrl) CTRL pull down resistor 典型值是800k欧,就想着不需要再串接一个限流电阻到输入电压了。

问题2:6串3并的设计,每一路的电流都要求是350mA,所以只有其中的一路接到了FB引脚上。如果3路都接到FB引脚上,按我的理解电流应该只有350/3=117mA了,所以只能像图上这样的接法。不知道这样的理解有没问题。

问题3:功耗核算。输入电压是12V,效率按85%,3串,12×0.35×3/0.85/18=0.82,输入峰值电流加上20%余量,为0.82*1.2=0.98A,小于芯片开关电流1.2A的限制,故理论上是可以行的。但看到其他帖子中TI工程师对开关电流的限制为0.96A,按照这个数字的话又是不可行的,那只能修改方案,改为两串了。3串究竟是否可行?20%的余量有没妥协空间?

问题4:如果FB引脚连接的LED灯串有一个没焊好或使用过程中故障形成了开路,则输出电压为38V,另外灯串LED避免不了被烧毁的结局吧?因为另外的灯串没有连接到FB引脚。

哪位大神有空指点一二,不胜感激。