This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2110A使用的问题?

Other Parts Discussed in Thread: TPS2110A

1.我使用TPS2110A的芯片单片机控制选择IN1和IN2的电压输出,如下图所示,如果我的IN1为3.3V,IN2为5V,此时设置DO=0,D1=1输出为IN2的电压5V时,看芯片的内部图是使用的MOS做开关切换的,这里是否有会5V反灌至IN1端的情况?

2.这个芯片的供电电源是来自IN1和IN2这里对电流是否有要求?我的有一路输入电流最大只有1mA是否满足?