This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930 DSG和CHG驱动电压问题

你好,我现在在做10对MOS并联驱动,涉及到驱动电压和驱动能力的问题,有几个疑问:

1. 可否用BQ的DSG和CHG引脚直接驱动10对MOS,会不会有驱动能力不足的问题

2. DSG和CHG引脚驱动电压是固定的还是什么,手册中只找到以下描述,我的电池电压比较低的时候,驱动电压也会跟着降低吗

3. 请问有什么办法提高驱动电压,或者维持在12V左右