如题,BQ2060A充满后(电池电压已经4.15V,已结束充电),但是指示灯只有两颗亮,这是为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,感谢回复!
我用的是2340容量的电芯,两并三串(即设计容量是2340*2=4680mAh)。
Last Measured Dsg设置为4680mAh
Pack Capacity设置为4680mAh
Cycle Count Threshold设置为4410mAh
要怎么样才可以发图片?可以的话我发EEprom界面上来帮忙看看有没有问题。
部分关键参数设置如下:
Fast Charging Current:2000mA
Pre-Charge Current:100mAh
Maximum Overcharge:300mAh
Overload Current:6000mA
Overvoltage Margin:304mV
Overcurrent Margin:512mA
Fast Charge Termination%:100%
Fully Charged Clear%:95%
Charge Effciency:100%
Current Taper Threshold:143mA
Current Taper QualVolt:200mV
Near Full:256mAh