现在需求带PWM调光的LED驱动电源,输入电源电压在200VAC置240VAC之间,电源需要隔离,输出电压最大60V,脉冲式输出,输出DUTY ON时间为100US至300US可调,周期200HZ,在DUTY ON时间里输出电流恒定为8A,可有什么芯片可以实现这个功能
请专家们指教或者推荐其他方案。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在需求带PWM调光的LED驱动电源,输入电源电压在200VAC置240VAC之间,电源需要隔离,输出电压最大60V,脉冲式输出,输出DUTY ON时间为100US至300US可调,周期200HZ,在DUTY ON时间里输出电流恒定为8A,可有什么芯片可以实现这个功能
请专家们指教或者推荐其他方案。谢谢