现在在做移向全桥变化器,打算用UCC3895,选择的开关管是IGBT,工作频率暂定为20Khz,麻烦问下,ucc3895的内部振荡器的工作频率fosc可以工作在40kHZ吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见UCC3895 datasheet: http://www.ti.com.cn/general/cn/docs/lit/getliterature.tsp?genericPartNumber=ucc3895&fileType=pdf
最小频率震荡为89kHz, 此时CT最大取880pF, RT最大取120k.
Hi
SYNC的门限电压见datasheet: http://www.ti.com/general/docs/lit/getliterature.tsp?genericPartNumber=ucc3895&fileType=pdf 第四页。
以及LOADSYNC = 3.9 kΩ and 30 pF in parallel
或者见datasheet第四十一页。
dyty 应该是50%.