This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐一款输出可调的开关电源

Other Parts Discussed in Thread: OPA564, LMR33630, LMR16030, TPS54341, TPS54160

计划用OPA564输出一款±8V,±1A多的可调电源,考虑运放输出低压时功耗太大,希望能找一款可调电源根据,当运放输出低压时降低供电电压以节省功耗。

希望能推荐一款。

系统设计的输入电压可以很灵活,从5V~30V都满足,所以不用考虑输入范围的问题,可以固定在比如+24V或者+12V。

要求:

1、Vo=4.5V~12V, Io>1A;

2、该电源可以改造成负电源输出,Vo=-4.5V~-12V,Io>-1A;

3、输出电压在4.5V~12V(或-4.5V~-12V)范围内,环路均稳定;

4、当OPA564输出2KHz,±8V正弦波时,Vo响应速率能跟上;(个人菜鸟,不懂得这个该怎么描述:我认为由于电源的输出电压跟随运放的输出的,所以电源的响       应速率必须比Vo要快才行,但是这个因素要考虑哪个参数呢?考虑电源的环路带宽吗?)

5、另外就是成本和体积,由于一块PCB板子上有几百片OPA564,每个OPA564都要配备二个电源,所以希望不要超过1.5usd。由于使用外部电感,体积一定要            小,开关频率最好能调节到上MHz,减小电感体积。

请问,这个方案可能吗?我也想了很久,实在拿不准其他方法。我选了以下几个电源:

1、LMR33630系列;(额外疑问:该系列电源不支持Forced PWM模式,当负载从轻载到重载响应时,是否会形成较大电压波动?)

2、LMR16030系列;(额外疑问:不是同步整流,下管为二极管,是否会影响OPA564输出正电压负电流(或者负电压正电流),因为二极管的电流只有一个方向)

3、TPS54341系列;(额外问题:eco-mode能配置成负压输出吗?该芯片外部补偿,是否针对每种输出电压都要额外预留一套补偿电路)

希望TI的专家能帮忙解惑,不胜感激!