This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About UC3843 & UCC3803

Other Parts Discussed in Thread: UC3843

The project used UC3843 with 12V power supply. Now  the  power  supply  is  changed to  5V, So IC changed to  UCC 3803.Only the IC is changed, and the peripheral circuit is not changed, The  Circuit  as  follows:

1>When  used   5V   power supply,  The output of the sixth pin is abnormal, and the third pin is the waveform above, the waveform as  follows:

2>When  used   5.5V   power supply,  The output of the sixth pin is normal,the waveform as  follows:

3>There is a board, the input voltage must reach 8.5V, and the sixth pin can be switched normally,the  waveform as  follows:

4>modify the working frequency from 100K to more than 900 K,the output of the sixth pin is   abnormal,the waveform as  follows: