This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F415 在 LCD 空调红外遥控器中的应用

Other Parts Discussed in Thread: MSP430F415, MSP430F413

摘要

空调红外遥控器是通常由两节碱性电池供电,通过 38KHZ红外载波调制与挂机或者柜机单向通讯的便携式设备。由于其成本低廉,低功耗等特点不仅在空调,还在其它家电及玩具等领域得到了广泛应用。基于便携及电池供电的要求,系统的超低功耗及可靠性设计是首要目标之一。本文针对应用中对低功耗,高集成度的要求,采用MSP430F415 超低功耗 MCU,实现按键扫描,LCD 显示,红外发送等完整功能。

目录

1 空调遥控器简 介.............................................................................................................................. 2

2 系统结构和整体方 案....................................................................................................................... 2

3 系统软硬件设 计.............................................................................................................................. 3

3.1 系统时钟分 配.......................................................................................................................... 3

3.2 软件功能模块设 计................................................................................................................... 4

3.2.1 按键扫描设计 .............................................................................................................. 4

3.2.2 红外载波及编码发送设计............................................................................................. 6

3.2.3 整机软件功能架构设计................................................................................................ 7

4 系统可靠性设 计.............................................................................................................................. 8

5 总 结.............................................................................................................................................. 11

参 考文档 .............................................................................................................................................. 1

下载观看:zhca425.pdf

作者:MSP430 产品技术支持工程师   郭君 

  • CPU MSP430F413/415 特性描述 ※ 低工作电压范围:1.8 V ~3.6 V ※ 超低功耗     活动模式:200μA at 1 MHz, 2.2 V      待机模式:0.7μA      关闭 (RAM Retention): 0.1μA ※ 五种省电模式 6μs内从待机模式唤醒 ※ FLL+时钟系统 ※ 16-Bit RISC 指令体系, 125ns指令周期 ※ 16位定时器TIMER_A带3捕获/比较寄存器(F412、F413) ※ 16位定时器TIMER_A带5捕获/比较寄存器(F415、F417) ※ LCD控制器/驱动器(多达96段) ※ 片内比较器欠电压检测器 ※ 带可编程电平检测的电源电压管理/监控(F415、F417) ※ 串行在线编程,无需外部编程电压,安全熔丝可编程代码保护