This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65218D0的DCDC1~4的寄存器配置,PFM功能初始状态是禁用状态还是启用状态?

Other Parts Discussed in Thread: TPS65218D0

TPS65218D0的DCDC1~4的寄存器配置,PFM功能初始状态是禁用状态还是启用状态?

现DCDC1和DCDC2的开关频率不安定,超出了DATASHEET提供±12%的偏差。考虑是不是进入到PFM模式的原因呢?

IC直接使用,没有进行再配置。DCDC1和DCDC2这两个通道的消费电流是6000mA.

求解答。

  • Hi
    默认PFM模式, 见DC/DCX寄存器配置。频率参数表给的是典型值,12左右的偏差虽然有些大,但是没有问题,频率这里最多也就稍微影响一点纹波电流了。轻载才是PFM模式,这里应该是规格tolerance的问题.
    DC/DC的最大电流到不了6A,注意,是否写错了。
  • Johnsin您好,感谢您的回复。消费电流是0.6A,之前记载有误。
    想再确认一下,当负载为0.6A的情况下,算是轻载吗?
    另外,DCDC1,DCDC2的负载是0.6A,开关频率超过了2400kHz±12%的范围。
    而DCDC3和DCDC4的负载分别是0.662A和0.642A,其开关频率却没有超出2400kHz±12%的范围,原因是什么呢?
    DCDC1~4,判定轻载的电流界限值分别是多大呢?
  • Hi
    看另一个回复。