Other Parts Discussed in Thread: BQ25886
使用BQ25886充电时,充电输出为8.2V,1.2A;充电过程中芯片温度较高,测试为55℃到60℃,此时效率约为82%(考虑存在一定的线缆损耗,实际效率会比82%略高);接近充满后,充电电压由8.2V变为8.0V,充电电流由1.2A逐渐变为0.2A左右,0.2A充电20分钟以上,STAT引脚一直是低电平,没有变为高电平(也就是说充电没有完成,还在充电)。
请问:
1.BQ25886背部有散热焊盘,且有地网络的过孔,工作时55℃以上的温度是否正常,效率是否正常(规格书介绍在某些限定条件下效率是93%)?
2.0.2A充电多久后能充满,STAT能变为高电平?