This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】并联电源

Other Parts Discussed in Thread: TPS54560, UCC39002, TPS54620

问题描述:

是否可以将2路电源并联使用,以提升负载输出能力? 例如2片5A输出能力的TPS54560直接并联实现10A输出能力?

解决方案:

通常是不行的,原因在于无法均流。强行并联,可能会导致一路电流过大,而另一路过小。轻则因为过载保护不稳定,重则直接烧电路。但是可以通过UCC39002之类的均流控制芯片强制控制2路或者多路电源实现均流。只是这样控制比较复杂,因此不被建议,而寻求一些电流控制方式的电源芯片,因本身特性能实现均流效果,相对电路会简单很多。

控制电路举例:

以TPS54620为例,这是一款峰值电流控制,最大6A输出的降压芯片,2片并联后可以实现12A的输出。注意2片芯片共用Comp, 同步信号180°相差。

 

参考文献:

https://www.ti.com.cn/cn/lit/pdf/slva389

E2E相关讨论贴:

https://e2echina.ti.com/question_answer/analog/power_management/f/24/t/143888

https://e2echina.ti.com/question_answer/analog/power_management/f/24/t/108353

https://e2echina.ti.com/question_answer/analog/power_management/f/24/t/51955