This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196输出电感啸叫



LED backlight circuit, output voltage 51V, each LED current 105ma. The current problem is that the output inductor l546 has been whistling. I try to adjust the FSW frequency and Iset current are useless, what is the solution. The inductance l546 is in accordance with the official recommended model.

LED背光电路,输出电压51V,每一路LED电流105mA。目前遇到的问题是输出电感L546一直在啸叫。我尝试调节FSW频率和ISET电流都没有用,请问有什么办法解决。电感L546按照官方推荐的型号。

  • Hi
    在电感L546的输入端建议加大电容(22uF或者47uF), 因为输入电压会因为输入电容不够而瞬态被拉低,会导致更大的输入电容以及电感峰值电流,可能导致电感饱和而发声。
    其次确认电感饱和电流是否足够,建议适当加大。
    输入端的耦合电感其实可以不要。