Other Parts Discussed in Thread: BQ500210, INA214
在BQ500210电路中(图1),发射端具有监测输入电压电流的功能,U3芯片INA214就起到这个作用。4脚IN+接VIN,5脚IN-接负载,也就是Q1的供电源,R33,C23,R32的作用是输入管脚滤波以及调整增益误差的计算,参考电压2脚接地实现无方向工作模式,6脚输出反应了4、5脚差分输入的变化。而Q1的D极电压由VIN经过电阻R7提供(Q1的D极电压也是发射电感的峰峰值电压)。在实验中,测量的结果VIN=19V,Q1的D极电压为18.9V,也就是图2中Vsupply与LOAD的电压比较接近。现有个问题不太明白,无线充电过程中,若接收端需要更多能量时,发射端通过改变发射频率就可以增加能量传输,而Q1的D极电压不会改变,INA214的输出也就没有改变,这如何起到监测电压电流。是不是我理解错了,请指教下电路中如何监测电压电流,麻烦解释详细点,期待你的回复,谢谢!

图1

图2

图3