This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池供电 正负15V 正负12V 正负5V 3.3V输出

Other Parts Discussed in Thread: MSP430F5529, TPS61093, TPS63900

为参加今年TI杯,想设计一款电源模块,要求可以给运放,AD,DA,MSP430F5529供电,请问有比较好的方案吗?

  • Hi
    AD,DA,MSP430F5529供电电流需求一般不大,你可以选择升压芯片加chargepump的方式来做,见TPS61093, TPS61080, 电流大的话选择TPS61081. 关于正负双输出电源电路,datasheet上都有参考,设计相对简单。
    对于给运放,或者AD供电,很多都要求noise 纹波尽量小,麻烦一点是在正负电源后增加一级LDO, 如果要节约成本的话,建议至少增加LC滤波。
    如果要3.3V的话,可以选择LDO,很多的,在TI LDO产品中看,太多了。稍微负载一点可以选择升降压DC/DC,这样电池可以工作到3V以下,例如TPS63900.