This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40211电源芯片boost升压的输出电压与WEBENCH参考电路上的不一致

Other Parts Discussed in Thread: TPS40211

TPS40211.TSC

这个电源电路是按照输入12V,输出48V 1.5A设计的。但是仿真实际输出只有22V,且发现FB的电压比芯片提供的范围要小,大约是113mv,请问有什么解决方法吗

  • Hi
    因为输出功率相对较大,建议你将输入电容适当放大一点,并且靠近电感输入端。功率电感饱和电流尽量大一点,建议8A以上。
    其次这个芯片驱动能力不是很强,注意选择尽量小Qg的MOS,建议增加驱动电路。