This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

调试3895时遇到问题,请教高手,帮忙解答,万分感谢!!!!!

1、我是在设计充电机的时候用到的3895,对电压模式、峰值电流模式和平均电流模式时3895的各种连接方法很是疑惑,我的原理图中不知是什么模式?采用该原理图我已经调制吃自己想要的波形,但是所采用的RT端电阻和CT端电容的值和理论计算出来的值出入很大!(我实际采用的电阻和电容的值是一个一个试出来的,而且在调试的时候发现,当增加电容值的倍数时,周期并不随着进行相应倍数递减,但是改变电阻的倍数时,周期就可以相应改变)请高手帮我解答这个问题,谢谢!!

2、当采用峰值电流模式控制时,要加入斜坡补偿,是不是CT端通过三极管跟随电路将信号送到RAMP端,就是一种补偿呢?如果不加斜坡补偿的话,其在占空比大于50%的时候会造成电压不稳定,就是电压波形占空比在这个周期大于50%,在下一个周期小于50%,是因为这个造成电压值不稳定的吧?对此我也画了逆变部分各个IGBT和电感中的电压电流图,如附图所示,改图最底下一个波形图就是我认为的在峰值电流模式控制下,电压占空比改变的具体分析图,不知我画的是否正确?

3、在调试的过程中,我发现在EAP输入电压等于0.71的时候,移相为20度,当小于0.71V时,移相值一下变到0度,不知道这又是为什么?如果这个合理的话,那么我想要的移相从0度到180度就不能够实现了,是不是?

4、在调试的时候我发现OUTA、B、C、D输出波形边沿都有冲击电压波,不知这能不能消除,该怎么消除呢,请求指点

图片.rar