This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27524驱动MOS怎样设置合适输出电压

Other Parts Discussed in Thread: UCC27524

您好!

如附件图,我想UCC27524 输出OUTA/OUTB分压3.4V,作为MOS的VGS,驱动MOS管CSD19506K ,考虑UCC27524输出,不知这样是否能驱动CSD19506K?

谢谢!

SCHEMATIC1 _ PAGE1.pdf

  • Hi
    MOS驱动是电压驱动型,但是要有较大的驱动电流,如果采用分压,电流会非常小,整个周期可能大部分时间用来做上升沿或者下降压,严重降低效率,而且严重影响占空比。所以都是直接驱动,不用电阻分压。
    如果驱动芯片的VDD远远大于MOS的Vgs,可以适当降低VDD(仍在其供电氛围内,实在不匹配就只能换芯片), 但是大部分的MOS管,Vgs耐压都是20V左右(包括CSD19506K),所以是可以直接驱动的,具体可以看一下驱动芯片的datasheet和MOS的datasheet。