为什么CHG 和 DSG 的电压都是参考VC2? 不是DSG 参考Vpack, 而CHG 参考 VC2吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
V(FETON)
Output voltage,
CHG and DSG on
VDSG(ON) = VDSG – VVC2, 4.07 V ≤ VVC2 ≤ 18 V, 10 MΩ
between PACK and DSG 8.75 9.5 10.25
V
VCHG(ON) = VCHG – VVC2, 4.07 V ≤ VVC2 ≤ 18 V, 10 MΩ
between VC2 and CHG 8.75 9.5 10.25
为什么都是VVC2呢?VDSG(ON)=VDSG-Vpack,这样才对的吧?