Other Parts Discussed in Thread: BQ24650
我的太阳能板参数:
峰值功率:20W
开路电压:21.6V
短路电流:1.14A
峰值电压:18.2V
峰值电流:1.1A
问题1:BQ24650的Vmppt的值是不是参数中的18.2V?
问题2:我如果用外接的12V电源通过BQ24650给9.6V的电池充电,能充进去电吗?
问题3:如果问题2可行,那么我希望我的电路既支持太阳能板充电,又能支持外部12V电源充电,这个Vmppt的值该设置多少才合适呢?
问题4:BQ24650具备VIN_DPPM功能吗?我看手册里面没有说明,但是我选型的时候选中这个特性里面有这个芯片