This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890H充电IC技术咨询

Other Parts Discussed in Thread: BQ25890H, BQ25890

Hi team

客户咨询一个问题,需要专家支持:

客户正在使用BQ25890H充电IC ,目前想实现方案,USB 5V500mA,标充5v2A,快充9v2A,,目前在使用9v2A充电过中 要求电池电压在3v-4.2v使用9v2A,电池电压超过4.2v切换为5v2A,这样可以提高充电效率,降低芯片问题,请问这个方案可以实现?还有INDPM 默认为3.9v,这个可以配置4.6v吗?

Best regards

Aosker

  • 您好,我查到的信息如下:
    For BQ25890/5:
    EN_HVDCP=0, vbus=5V,
    EN_HVDCP=1 and EN_12V:0 results in VBUS=9V with HVDPC adapter.
    EN_HVDCP=1 and EN_12V:1 results in VBUS=12V with HVDPC adapter.
    For BQ25890H,
    default settings of EN_HVDCP=1, EN_12V=0 results in in VBUS=9V with HVDPC adapter.
    电池电压在3v-4.2v使用9v2A,电池电压超过4.2v切换为5v2A需要却换成非HVDPC adapter
    INDPM 参数配置请参考数据手册47页表21. REG0D