This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138 DPWM三角模式问题



请问:在三角模式中,DPWM B Rising Edge的值能否超过中心点(Period/2)?

例如: Period=16000 , Filter Duty=200 , Cycle Adjust A=200 , Cycle Adjust B=200

Dpwm1Regs.DPWMCTRL0.bit.D_ENABLE = 0;

Dpwm1Regs.DPWMCTRL0.bit.PWM_B_INV = 0;

这个时候计算出来的: DPWM B Rising Edge = 8100 , DPWM B Falling Edge =7900

这样DPWM输出的占空比是不是就变成 98.75%?还是输出0%?