上图为LM3485的典型应用,不知道是否可以通过da输出一个基准电压来控制lm3485实现0-35V线性输出的电源?这个基准电压以何种方式来接进来最好?
不知道是否可以通过串接一个电阻接到FB管脚上来实现?可是理论好像无法满足输出范围?有没有更好的方法?
谢谢@!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果要输出连续可调的方法,最好使用MCU或C2000控制,或者使用数字电源芯片如UCD3138, UCD9XXX的芯片来做。
如果是BUCK芯片,要线性输出,并且输出电压范围这么宽的话,估计很难做到。
一般使用LM10010芯片这样的DAC,通过I2C来控制调整输出,但只能是步进调压,并且调压范围一般比较小。
谢谢,数字电源芯片这些估计对于系统来说比较复杂了,我还是希望采用单片机控制DA芯片,通过输出基准电压,串一个电阻接到FB,这种方式,不知道是否可行?可调范围一般是用到10-30v之间。或者有那些buck芯片可满足全范围调节的?