This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z80 MaxTurboPwr() SusTurboPwr()

Other Parts Discussed in Thread: BQ40Z80

最近有在BMS中输出SOP(State Of Power)信息的需要。

对于bq40z80 TRM 手册中的第152页中的MaxTurboPwr() 和SusTurboPwr()有以下疑问:

1、MaxTurboPwr()是不是电芯的最大功率输出值,而SusTurboPwr()是不是电芯允许的持续功率输出值?

2、如果想要在BMS中输出SOP信息值,是否可以直接使用这两个值作为输出?

谢谢!

  • 您好
    1, 这两个参数的介绍请参考下面的内容.
    MaxTurboPwr() This command reads the maximal peak power value for 10-ms pulse occurring on top of 10-s 2 C-rate pulse.
    SusTurboPwr() This command reads the maximal peak power value for 10-s pulse, sustained turbo power, in cW
    We do not recommend using Turbo Mode for non notebook applications.