如题,请高手回复,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,请高手回复,谢谢。
输入电流肯定是断续的,也正因为这样,所以THD比较难做
allen Leung1 说:300W buck pfc? pfc是ccm还是DCM mode?
david cheung 说:您好,最近比较忙,此项目目前样品板,基本焊接完毕。可否留下电话,为以后调试方便做基础。可否留下联系方式,谢谢。
你留个邮箱吧。
最后,PF值只能调到0.86,调不上去了,只能减小前面的X电容,功率因数才可以达到0.95。 聚丙烯响的问题没有解决;所以换BOOST PFC电路了,截止今天,通报BOOST PFC的结果。 480Vac输入,功率因数0.98,输入功率260.5W,无极灯正常启动,都没有问题。开路、短路保护都可以,功耗也在预期范围内。只不过就是的购买900V的mos管,有点贵。