This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH12040W调压

Other Parts Discussed in Thread: PTH12040W

请问下,现在有一个应用场景,默认负载侧电压0.85V,电流40A左右,系统是2米长距离供电,DCR=40毫欧,路径上的损耗大概是1.6V。

目前需要寻找一个电源模块,需要支持0.8V~3.3V输出,电流40A.找了下TI的电源模块有一个PTH12040W模块支持以上应用,但是不知道如何通过负载的变化自动调节输出端电压,即:轻载时,模块输出电压在0.8V,满足时模块输出电压为2.4V。

请教下论坛中的各位,如果需要增加外部电路控制,该如何实现呢?或者说,是否可以控制Vo Adjust管脚实现上述需求呢?

  • Hi
    像这种情况比较建议你将电源板块放到负载端,那么消耗就是输入了。
    放到输出,线损实际上并不很确定,而且很难将线损设计到反馈中。(除非2根线,一个带负载,一个做反馈,但是2米长的反馈,这个又容易引入噪声。所以建议你将电源板块放到负载端。