This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS43061电流检测电阻选择的问题

Other Parts Discussed in Thread: TPS43061

各位老师

       关于TPS43061的电流检测电阻,在技术手册和设计工具中最后给出的都是使用两个并联的电阻,例如计算出来电阻需要9.89mΩ,参考设计中会使用两个20mΩ并联的方式,而不是只使用一个10mΩ的电阻,对于这点不是特别理解,是否就是因为这样选择可以降低对电阻功率的要求,从而减小电阻体积,还是说有别的考虑,望解答,万分感谢!

  • Hi
    选择sense电阻除了感值,还要考虑sense上的功耗,例如2A的电流,流过10mohm, 功耗是40mW, 但是分2个20mohm, 每个值消耗10mW. 而一般10mohm和20mohm的额定功率是一样的。所以电流大,一般是2个电阻并联,甚至更多。