This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5017输出电压问题



如图所示设计。目标电压值24V,当设计输入30~47V,当输入30V时,输出只有8.7V,当输入47V时,输出0V,这是什么愿意

  • 设计电路是这样,输入电压DC30~47V,输出目标电压24V,但是当我输入30V时输出电压是8.7v,输入47V时输出电压0v,这是怎么回事

  • Hi
    首先你要确认你的功率电感饱和电流是否是最大峰值输出电流的1.3倍以上。因为如果电感饱和容易造成输出电压拉低。而且在输入电压增高时这种现象会恶化。
    其次要注意layout, 特别是功率回路,如果layout不好,导致带载能力下降也是会导致输出电压拉低的。
    如果上面都没有问题,你可以将电路通过下面“使用高级编辑器编辑文本”中的插图方式将电路贴上来看看。