This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教bq24075输出问题

Other Parts Discussed in Thread: BQ24075, BQ24079, LMR62421, BQ24090, LM4510, BQ24195

我看bq24075数据手册,上面关于OUT的介绍:System Supply Output. OUT provides a regulated output when the input is below the OVP threshold and above the regulation voltage. When the input is out of the operation range, OUT is connected to VBAT except when SYSOFF is high (bq24075 and bq24079 only). Connect OUT to the system load. Bypass OUT to VSS with a 4.7 μF to 47 μF ceramic capacitor。想问一个问题,当输入没有时,只写到OUT is connected to VBAT except when SYSOFF is high 不知此时out输出电压是否稳定。我们的系统需要有适配器供电时稳压到4.5-5.5v和适配器掉电时由电池供电稳压到4.5-5.5v,如果bq24075不能实现,麻烦推荐一个型号或方案,不胜感激。

  • 当适配器没有的时候,系统输出端直接连接BAT pin,不具备调整能力,所以此时的输出电压就是电池的端口电压,而单节锂电池达不到你的需要的稳定在4.5-5.5V要求,所以根据你的需求应该在OUT端加一级电压转换电路,假定你使用的是锂电池,那么可以用一个支持从4.2V升压到5V(接近15%这样比较小占空比)的boost电路(即Boost电路的最小on时间能够得到保证)得到你需要的电压,由于boost电路的架构特性,当输入电压高于输出电压的时候,此时输入电压会通过电感和续流二极管直接加到输出端,所以BQ24075在适配器插入时,通过电感DCR和续流二极管的压降,在输出端也能得到接近5V的电压。

    因此若适配器的输出电压高于5.5V(即保证适配器电压经过BQ24075的output输出后,电压经过电感和二极管还能有高于最低4.5V需求的电压余量),输出电流不大,续流二极管的功耗可以接受,建议你可以考虑LMR62421这样的升压转换器接到BQ24075的系统输出端,设定LMR62421的输出电压为固定的5V ,真正的负载接LMR62421的输出。

  • 谢谢您的回答,我们使用的是锂电池(8400mAH),反正要升压转换器所以不需要BQ24075,那么我想用bq24090就可以给锂电池供电,LMR62421升压转换器接到BQ24090的系统输出端,这样配置是否可行?我们的负载电流不超过200mA,请问升压转换器可以用LM4510吗?还有想问一下有没有单片解决方案?

  • 由于你的电池的容量比较大,所以如果选用1A最大CC模式的充电器会导致充电的时间非常的长,因此采用开关模式的充电器能支持更大的CC模式的充电电流使得充电的效率更高,此外需要注意充电器的选择需要考虑到电池的化学类型,锂电池电池 ,锂聚合物电池,还是磷酸铁锂电池需要选用对应的充电器,

    如果满足BQ24090x芯片对于并联负载的要求(A system load can be placed in parallel with the battery as long as the average system load does not keep the battery from charging fully during the 10 hour safety timer),那么您可以选用BQ24090

    后端升压芯片的选择在你的这个项目中需要考虑到最小占空比的要求是否被支持,以及内部的集成开关允许的最大电流是否足够(一般为Ioutmax*1.2*Vout/Vin,这里要考虑到最恶劣的情况,即Vout取最大,Vin取最小)

    对于你的要求建议也可以考虑BQ24195这个比较新的针对power bank开发出来的器件,它具有路径管理,同时也有PMID这个升压架构稳定输出到5.1V。可以配置为默认的不需要主机i2c控制的独立工作模式。