Other Parts Discussed in Thread: LM46002
一个车用的产品,DCDC采用的LM46002,输入电压12V,输出5V,经二极管后输出4.8V供给后级的CAN芯片,负载电流只有几毫安。详细电路及PCB见下图。
生产了1000片,在工厂生产的时候,有20片出现一上电CAN芯片就损坏。
CAN芯片采用的NXP的TJA1051T/3,把损坏的芯片寄原厂FAE分析,为电源(4.8V)脚供电异常导致,下面最后的图片为CAN芯片原厂FAE的测试结果。
但是在4.8V电压上,用示波器测量电压很稳定,开关机也没有脉冲。
进行破坏性测试,将CAN芯片电源脚电压不断提高,电压到12V时CAN芯片才损坏。
然后又对其中30块板子进行了老化测试(通电30秒--断电30秒--通电30秒。。。。。。),每块板子重复了300次,也没能将故障重现。在这20块板子损坏之后,无法再重现损坏CAN芯片的现象。
请帮忙确认:
1.下图中的电路设计及PCB Layout是否有问题?
2.负载过低的情况下(1mA),是否会导致电源不稳定?
3.电源没有测试到脉冲的情况下,还会有其它原因导致后级芯片损坏吗?