请教一下普通三端稳压比如LM317 LM350和LDO的输入输出电容正确的配置计算方法,总感觉书上讲的不完整或者不对,是不是用去耦电容的计算方法比较准确 正确一点,比如LM350带宽是10-10KHZ,输入部分需要对10-10khz去耦,让它在10-10KHZ良好工作,负载的带宽大于10KHZ,所以输出部分需要对于10KHZ以上电流进行去耦补偿
比如稳压芯片用LM350,负载最大电流是2A,变压器是次级是9V的环形变压器,用全桥整流,滤波只用电容,该怎么设计才能发挥最佳性能呢,如果输入去耦到20HZ,输入电压波动小于2.5%,需要50000uf左右的滤波电容,1khz需要1000uf,10khz需要100uf