This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792 SYS輸出不穩定

Other Parts Discussed in Thread: BQ25798

我們使用貴司BQ25792設計一款電池充電線路,現出現以下問題:

1.僅使用VBUS供電,SYS輸出不穩定,電壓會跳變,抓取的SYS波形如附件:

3005.waveform.xlsx

2.僅使用Battery(Vbat>3.5V)或VBUS + Vbat(Vbat電壓>3.5V,REG00寄存器SYS設置使用默認值)供電,SYS輸出是穩定的

這種情況一般是什麼原因造成的?線路設計如附檔,請幫忙協助確認下,感謝~~~~~

8132.BQ25792.pdf

  • 您好,正在查询,稍后回复。
  • 您好,BQ25792的设计预期是,当卸下电池时,要么通过CE位/引脚禁用充电,要么卸下的热敏电阻将导致TS故障并禁用充电。 在使用VBUS且没有电池的情况下,充电电流快速打开,从而导致BATOVP故障,然后导致SYSOVP故障。 故障然后使转换器停止。 在BAT(470uF)处添加大电容通常可以防止OVP事件。

    具有相同引脚输出的即将发布的BQ25798改变了故障时序,因此转换器不会关闭。