电源输入从9V逐渐加到15V时,芯片突然烧了,设计是按照TI的WEBENCH设计的,就是电感更换了型号,电感值还是一样的,MOS管按照推荐来的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电感感量还好,略有偏差没有问题,但是一定要注意饱和电流。按照你1A的输出来选择。因为带的是感性负载,建议你将输出电容尽量加大一点。
如果只是输出电容的问题,能导致芯片烧了嘛?这个芯片加MOS管是否能满足我的需求,输入从9V-15V任意电压输入,输出始终保持12V,最大1A电流的输出?
麻烦请帮我看看原理图和PCB板有什么问题嘛?非常感谢!LM3488.docxSOLASE_12V-V1.0.pdf
Hi
芯片哪个脚烧? 电流异常应该烧MOS的,主要看一下功率电感饱和电流。
电路直接借助webench仿真就可以得到,PCB layout主要注意功率回路小一点,以及输入电容靠近电感端。