您好,选择TI公司的LP5900,为了防止下电过程中LP5900的输出端电压下降速度慢于输入端(输出端有100uF电容),导致电流反向灌入,通常并联一个二极管,阳极接输出端,阴极接输入端。想知道这个二极管选择开关二极管,稳压二极管,还是肖特基二极管呢?
关注哪些指标呢?反向电压大于输入电压,正向电流多大合适呢,需要额定功率是多少?
实际工作情况:输入端5V,输出端1.2V~3.3V,输出端电容100uF,LP5900最大输出电流150mA
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,选择TI公司的LP5900,为了防止下电过程中LP5900的输出端电压下降速度慢于输入端(输出端有100uF电容),导致电流反向灌入,通常并联一个二极管,阳极接输出端,阴极接输入端。想知道这个二极管选择开关二极管,稳压二极管,还是肖特基二极管呢?
关注哪些指标呢?反向电压大于输入电压,正向电流多大合适呢,需要额定功率是多少?
实际工作情况:输入端5V,输出端1.2V~3.3V,输出端电容100uF,LP5900最大输出电流150mA
谢谢!
谢谢您的回答,您说的1A是正向连续电流(IFM)吗?想知道这个数值和LDO的实际输出电流有关系吗?因为尺寸受限,考虑IN4148WT(高速开关二极管,IFM=250mA, VRM=80V) 是否可以?
Hi
1A的推荐是我之前看到其他LDO增加的肖特基规格,因为这里实际上都是像输入电容充电,所以选择都应该差不多。电压很低,主要是电流。1A应该是最大脉冲电流。